Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IServer Interface / GetCurrentServerTime Method


GetCurrentServerTime Method
Retrieve the current Historian server time expressed in UTC.
Syntax
Function GetCurrentServerTime() As System.Date

Return Value

The current server time.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also