Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IServer Interface / GetSecurityGroupMembership Method



In This Topic
    GetSecurityGroupMembership Method
    In This Topic
    Retrieve the standard Historian security groups in which the currently authenticated user holds membership.
    Syntax
    'Declaration
     
    Function GetSecurityGroupMembership() As HistorianGroupMembership
    'Usage
     
    Dim instance As IServer
    Dim value As HistorianGroupMembership
     
    value = instance.GetSecurityGroupMembership()
    HistorianGroupMembership GetSecurityGroupMembership()
    HistorianGroupMembership GetSecurityGroupMembership(); 

    Return Value

    The
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also