Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IntegerCriteria Class / EqualTo Property



EqualTo Property
Syntax
'Declaration
 
<DataMemberAttribute("EqualTo")>
Public Property EqualTo As Integer
 
'Usage
 
Dim instance As IntegerCriteria
Dim value As Integer
 
instance.EqualTo = value
 
value = instance.EqualTo
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also