Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IntegerCriteria Class / NotEqualTo Property



In This Topic
    NotEqualTo Property
    In This Topic
    Syntax
    'Declaration
     
    <DataMemberAttribute("NotEqualTo")>
    Public Property NotEqualTo As Integer
    'Usage
     
    Dim instance As IntegerCriteria
    Dim value As Integer
     
    instance.NotEqualTo = value
     
    value = instance.NotEqualTo
    [DataMember("NotEqualTo")]
    public int NotEqualTo {get; set;}
    [DataMember("NotEqualTo")]
    public:
    property int NotEqualTo {
       int get();
       void set (    int value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also