Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmInfo Class / Severity Property



In This Topic
    Severity Property (AlarmInfo)
    In This Topic
    Syntax
    'Declaration
     
    <DataMemberAttribute("Severity")>
    Public Property Severity As UInteger
    'Usage
     
    Dim instance As AlarmInfo
    Dim value As UInteger
     
    instance.Severity = value
     
    value = instance.Severity
    [DataMember("Severity")]
    public uint Severity {get; set;}
    [DataMember("Severity")]
    public:
    property uint Severity {
       uint get();
       void set (    uint value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also