Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmInfo Class / NumVendorAttributes Property



In This Topic
    NumVendorAttributes Property (AlarmInfo)
    In This Topic
    Syntax
    'Declaration
     
    <DataMemberAttribute("NumVendorAttributes")>
    Public Property NumVendorAttributes As Integer
    'Usage
     
    Dim instance As AlarmInfo
    Dim value As Integer
     
    instance.NumVendorAttributes = value
     
    value = instance.NumVendorAttributes
    [DataMember("NumVendorAttributes")]
    public int NumVendorAttributes {get; set;}
    [DataMember("NumVendorAttributes")]
    public:
    property int NumVendorAttributes {
       int get();
       void set (    int value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also