Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmField Class / Select Property



In This Topic
    Select Property
    In This Topic
    Syntax
    'Declaration
     
    <DataMemberAttribute("Select")>
    Public Property Select As Boolean
    'Usage
     
    Dim instance As AlarmField
    Dim value As Boolean
     
    instance.Select = value
     
    value = instance.Select
    [DataMember("Select")]
    public bool Select {get; set;}
    [DataMember("Select")]
    public:
    property bool Select {
       bool get();
       void set (    bool value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also