Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmField Class / OrderPriority Property



In This Topic
    OrderPriority Property
    In This Topic
    Syntax
    'Declaration
     
    <DataMemberAttribute("OrderPriority")>
    Public Property OrderPriority As Short
    'Usage
     
    Dim instance As AlarmField
    Dim value As Short
     
    instance.OrderPriority = value
     
    value = instance.OrderPriority
    [DataMember("OrderPriority")]
    public short OrderPriority {get; set;}
    [DataMember("OrderPriority")]
    public:
    property short OrderPriority {
       short get();
       void set (    short value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also