Generate an Equipment Model for Web HMI

You can generate an Equipment Model CSV file from Workflow data that can then be uploaded to Web HMI.

About this task

You can select equipment items to be excluded from the CSV file prior to generation. Once generated, the saved CSV file can be edited and uploaded to the Web HMI application.

Procedure

  1. In the navigator, select Proficy System > Proficy System.
  2. From the Displays panel, select HW/SW > Generate Operations Hub Model.
    The Generate Operations Hub Model page appears.
  3. Set up a path for a new CSV file as follows:
    1. Under Configuration, click the ellipsis () for the Output File Path field.
    2. Navigate to a folder on your local drive.
    3. Enter a name for the CSV file after the path in File Name.
    4. Select CSV File (.csv) (*.csv) in the Save as type field, and then click Save.
      The selected path appears in the Output File Path field.
  4. Optional: If you want to exclude any portion of the Equipment Model in your generated file, do the following:
    1. Click Select.
      The Universal Browser appears.
    2. Navigate through the columns and select one or more items from the hierarchy to exclude.
      Tip:
      Use Shift+click to select continuous items or Ctrl+click to select individual items.
    3. Click OK.
      The item(s) appears next to Select.
      Note:
      If you want to remove an equipment item from the exclusion list, click the X next to the item.
  5. Click Generate.
    The model file successfully generates and opens on the desktop.