Configure access to specific equipment instance details
You can configure your environment to allow members of certain personnel groups to view the details of only specific equipment instances or levels of the equipment hierarchy from the S95 Model Editor.
About this task
- When group members have permissions on an equipment instance, they also have the equivalent permission on its child instances.
- When group members try to access levels of the equipment hierarchy that they do not have the Read Equipment permission for, a message is displayed in the S95 Model Editor stating that the user does not have permission to view the details of that equipment.
Note:
Any changes you make to a group's key sets take effect the next time the members
of the group log in.
Procedure
-
If you are configuring a new key set, start here. If you are using an existing
key set, skip to step 2.
- In the navigator, click , and then select the group you want to configure.
- In the Displays panel, click .
- Click Assign Key Sets.
- In the Select a Group area, select the group that you want to configure.
- In the Permission Details For area, select the Edit by Key Set option.
-
In the Edit by Key Set area, under the System
Visibility key set:
Click... To... Add Workstation Add a specific workstation to the key set for the selected group. Add All Workstations Add all workstations in the system to the key set for the selected group. - Click Save.
-
In the navigator, select
, and then navigate to and select the equipment instance that you
want to provide access to.Note:You can configure access for multiple instances and at various levels; for example, you can configure access to a single production line at one site and all levels of the hierarchy at another site.
- In the Displays panel, click .
- In the Select a Group area, select the group you are configuring equipment access for.
- In the Permission Details For area, select the Edit by Key Set option.
-
In the Edit by Key Set area, under the Equipment
Configurator key set or another key set that you created for this
purpose:
Click... To... Add Workstation Add a specific workstation to the key set for the selected group. Add All Workstations Add all workstations in the system to the key set for the selected group. -
Click Save.
Note:The group members can access the selected instance and its child instances.