Email Server Configuration
You use the Email Editor to manage the email server configuration. From the email server, you can send out emails from a particular sender automatically.
- In the navigator, click .
- From the Displays panel, select to display the Email Configuration Setup page.Note:The Email Configuration Setup page appears.
- Enter information into the following fields, and then click Save.
Property | Value | Description |
---|---|---|
Server host name | User-defined | Specifies the host name or IP address of the SMTP server. |
Enable SSL | N/A | Enables SSL encrypted communication to SMTP server. |
Server port number | User-defined | Specifies the SMTP server's port number. |
Anonymous | N/A | Select this option if you have anonymous access to the server. Selecting this option disables the User Name and Password entries. |
User/Password | N/A | Select this option if you want to use user authentication when sending an email message. |
User Name | User-defined | Account user name used to authenticate to SMTP server. |
Password | User-defined | Account password used to complete authentication to SMTP server. |
Server timeout value | User-defined | Enter the number of seconds allowed to connect to the SMTP server before timing out. |
Default sender address | User-defined | Enter the email address from which all emails will be sent. |
Default sender name | User-defined | Optional: Enter a name related to the email account from which emails are being sent. |
Test recipient email address | User-defined | Enter a recipient's email address in order verify the email server configuration. |
Send Test Message | N/A | Click this button to test the email server configuration settings. If the configuration is correct, the recipient will receive a message from Workflow Server. |