Units
A unit resource represents an alternate
production path within a process cell.
In the equipment model, a unit is a terminating resource; that is; the last resource in a hierarchy. Unit resources are contained within a process cell only when some variability exists within the process cell regarding the path a product takes. For example, a unit adds value to a process cell by adding a dye or chemical to the overall process.
The following information describes the hierarchy of this resource:
Required: | no; optional |
Contained by: | Process cell; Production unit; Unit |
Can Contain: | one or more Units; Equipment modules |
Details Tab
Attribute | Value | Description |
---|---|---|
Name | Required; user-defined up to 50 characters | Specifies a display name for a resource. |
Description | User-defined up to 255 characters | Provides more information about a resource that a user may find helpful. |
Properties Tab
For more information see Equipment Properties.
Classes Tab
For more information, see Equipment Classes.