Enterprises
An enterprise resource represents
a complete production organization and is the highest level resource in the equipment
hierarchy.
Enterprises are independent because they are not subordinate to any other resource
and they are the originators of production planning for a coordinated group of sites
or areas.
Note:
Within the enterprise resource, you must have a site defined where
child resources are configured to further define your process.
In the equipment model, the enterprise is the topmost resource, and must contain at least one site resource.
The following information describes the hierarchy of this resource.
Required: | one or more |
Contained by: | (none) |
Contains: | one or more Sites |
The following sections describe the information and properties available on each of the tabs on the S95 Editor for equipment resources.
Details Tab
You can change the name and description of this resource.
Attribute | Value | Description |
---|---|---|
Name | Required; user-defined up to 50 characters | Specifies a display name for a resource. |
Description | User-defined up to 255 characters | Provides more information about a resource that a user may find helpful. |
Properties Tab
For more information see Equipment Properties.
Classes Tab
For more information, see Equipment Classes.