Material Inventory

The Inventory View provides read-only information on material definition quantities in lots and descendant sublots associated with material definitions and equipment resources.

The following table describes the properties available in the Inventory View.

Note:
The Inventory View displays lots associated with a selected material definition or equipment model. Sublots appear under their associated lot only, even those with different equipment model associations.
PropertyDescription
S95 ID Specifies the name of a lot or sublot.
Description Specifies the description of the lot or sublot.
Material Definition Specifies the material definition that is associated with the lot.
Note:
All sublots must share the same material definition as their parent lot or sublot.
Location Specifies the equipment resource associated with the lot or sublot.
Status Specifies the state of the lot or sublot and associated resources.
Quantity Specifies the quantity of the material in the lot or sublot.
Note:
Lots and parent sublot quantities are not the sum of all child sublot quantities. All quantities of lots and sublots are independently set.
UoM (Unit of Measure) Specifies the unit of measure for the quantity of material.
Note:
Sublots can have different units of measure than their parent lot or sublot.

Properties For

You can view the associated material definition properties of a lot or sublot in the Properties For panel. The S95Id of the selected lot or sublot appears in the panel heading.

Click the arrow button to show or hide the panel.

The following table describes the property attributes that are visible:

Attribute NameDescription
Property Name Specifies the display name for a resource property.
Value Specifies the value of the property.
Units Specifies the unit of measure for the property, such as gallons, inches, or tons.