Event View
The Event View displays multiple active condition and time events in the Proficy System and the resources that currently are attached to the events.
Overview Tab
The following table describes the available options.
Attribute | Value | Description |
---|---|---|
Event List | User-defined | Displays a list of the active condition and time events, and indicates the quantity of each. Events can be sorted and grouped by name, event type, or logging enabled status. |
Refresh | N/A | Click to retrieve the current set of events. |
Subscribers | User-defined | Displays a list of resources that subscribe to the selected event. |
Start Logging/Stop Logging | N/A | Click to start and stop logging event information. |
Event Log Tab
The Event Log tab displays all the currently enabled events that have been triggered. This log lists up to 200 events; the oldest events drop off the list as new ones are added.
The following table describes the available options.
Attribute | Value | Description |
---|---|---|
Clear Log | N/A | Click to clear the event log. |
Name | User-defined | Displays the name given to the event when it was created. |
Timestamp | N/A | Displays the local time that the event was triggered. |
Property List | N/A | Displays all properties, such as variables, of the event. |