Add properties to a resource

Procedure

  1. In the navigator, click Equipment > Instances.
  2. Continue selecting from the lists that appear until you find the resource you want to work with.
  3. In the Displays panel, select an editor.
    The editor appears in the workspace, displaying the resource information.
  4. Click the Properties tab, and then click Add Property.
  5. In the Name field, enter a name for this property.
  6. In the Type field, select a data type or browse for a class.
    Note:
    If you selected an equipment class as the data type, you must expand the property to view the class properties.
  7. In the Value field, enter a value for the selected data type.
  8. If applicable, in the Unit of Measure field, enter a unit of measure for the selected data type.
  9. To bind the property to an external data source, do the following:
    Note:
    You cannot bind equipment class properties to an external data source.
    1. Select the Linked check box.
    2. Click in the Value field, and then click the ellipsis button.
      The Configure Data Source dialog box appears.
    3. Configure the data source, as required.
    4. If applicable, click the Show Details button, and then click Test external data link to test whether the data source is valid.
  10. In the Description field, enter a description for this property.
  11. Click Save.