Storage Units
A storage unit resource
represents an inventory of a specific material, a group of materials, or a specific type of
storage.
The physical location of a storage unit can be dynamic, such as when a specific material inventory is en route to a new location. A storage unit is a terminating resource; that is, the last resource in a hierarchy, and is generally applied when detailed inventory organization is needed.
The following information describes the hierarchy of this resource:
Required: | no; optional |
Contained by: | Storage zones; Storage units |
Can Contain: | one or more Storage units; Equipment modules |
Details Tab
Attribute | Value | Description |
---|---|---|
Name | Required; user-defined up to 50 characters | Specifies a display name for a resource. |
Description | User-defined up to 255 characters | Provides more information about a resource that a user may find helpful. |
Properties Tab
For more information see Equipment Properties.
Classes Tab
For more information, see Equipment Classes.