Order the properties in the properties tab

Procedure

  1. In the navigator, click Equipment > Instances.
  2. Continue selecting from the lists that appear until you find the resource you want to work with.
  3. In the Displays panel, select an editor.
    The editor appears in the workspace, displaying the resource information.
  4. Click the Properties tab.
  5. In the name field of a property with sub-properties, click the expand/collapse arrow to show or hide the sub-properties.
  6. Click in the title field for a column.
    Note:

    When the grid is sorted by anything other than name, the property names are fully qualified; each property and sub-property has its own row with no hierarchy visible. When displayed as fully qualified, no property can be expanded to show sub-properties or closed to hide sub-properties.

    The properties are organized alphabetically in that column.
  7. Click the same column title again to reverse the order of the properties.
    The ordering of properties is replicated for all equipment and equipment class Properties tabs.