Equipment Duplication
While Workflow allows for infinite levels of equipment in its hierarchy, Plant Applications has only three levels in the equipment model.
Workflow | Plant Applications |
---|---|
Enterprise | No equivalent |
Area | No equivalent |
Process Cell | Department |
Production Line | Production Line |
Production Unit | Production Line |
Storage Zone | Production Line |
Any equipment below | Production Unit |
When you try to duplicate a production unit or other equipment instance lower in the hierarchy from within the navigator, it can result in an aspect error because the children are moved to the same level as the original instance and this may result in duplicate names.
To avoid this when duplicating an equipment instance, you can specify a prefix to be applied to the names of all duplicated child equipment to ensure unique names in the model. For example, if you specify a prefix of ‘xyz,’ the child equipment will be named xyzChild1, xyzChild2, and so on. This extends all the way down the equipment hierarchy.
To not use a prefix, leave the prefix field empty.