Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ArchiveStatistics Class / FreeSpaceMB Property



In This Topic
    FreeSpaceMB Property
    In This Topic
    The available free space in the current archive expressed in MB.
    Syntax
    'Declaration
     
    <DataMemberAttribute()>
    Public Property FreeSpaceMB As UInteger
    'Usage
     
    Dim instance As ArchiveStatistics
    Dim value As UInteger
     
    instance.FreeSpaceMB = value
     
    value = instance.FreeSpaceMB
    [DataMember()]
    public uint FreeSpaceMB {get; set;}
    [DataMember()]
    public:
    property uint FreeSpaceMB {
       uint get();
       void set (    uint value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also