Viewing the Device Summary

In the device summary page, you can view device details, including device ID, technician assignment, health status, and resource usage.

Procedure

  1. In the left navigation pane, select Device Manager > Devices.
    The Device Manager page appears.
  2. In the device list, click a device name.
    The device's Summary page appears. The Summary page displays the following device details:
    FieldDescription
    DeviceIncludes information about the device, such as:
    • ID – unique ID assigned to the device.
    • OS – operating system the device is running on.
    • Assigned to – the technician the device is assigned to.
    • Enrollment type – displays the enrollment type (certificate or OAuth).
    • Container enabled – shows whether the device is enabled for containers.
    • First seen – timestamp of the first time the device connects to Edge Manager.
    • Description – brief description of the device, if given.
    • Location information.
    • Created by – name of the user who added the device to Edge Manager.
    ModelInformation about the device model, such as description, processor, memory, and storage.
    HealthDevice status (for example, "online" or "offline"), the last status change, time since the device was last restarted, and the polling interval (the time interval set to synchronize device data with the database).
    Note:
    If the System Up Time for the device is displayed as "Unknown," this indicates there may be a clock issue with the device. See Predix Edge Manager Common Errors for more details.
    Alert PolicyDisplays the associated alert policy for the device (if one is used).
    Resource UsageCPU, memory, and disk usage for the device.
    Note:
    CPU and memory utilization is not supported on Windows.
    Power Supply StatusDisplays the power supply type, the state of the power supply (charging, discharging), percentage of how full the power is, and the description if applicable.
    Note:
    Percentage Full and Description are optional, so they are only displayed for certain power supply types, such as battery.

    Power supply type and state are always displayed for each power type.

    If there is no power supply "Not available" displays.

    WirelessDisplays the wireless connection status.
    BluetoothDisplays the device's Bluetooth connection status.
    VPN VPN client information for the device, including client ID, public IP, IPv4 (internet protocol version 4), and IPv6 (internet protocol version 6).
    ConnectivityNumber of SIM cards associated with the device, ICCID (integrated circuit card identifier), IMEI (international mobile equipment identity), carrier, provider, and status.

    If there is a SIM card associated with the device, you can click the ICCID link to view the details for the SIM card.

  3. (Optional) Click Edit to update the following:
    • Device name
    • Device model
    • Assigned technician
    • Description
    • Location information
    • Custom attributes
    1. Click Finish to save the changes.