Predix Edge Manager Common Errors
The following are general issues you may experience when using Edge Manager.
500 Internal Server Error When Importing Device List
500 Internal Server Error
Failed to upload the devices. An unexpected error has occurred, try again later.
Cause
The device list may not meet the required format.
Solution
- The file is a valid CSV file with a .csv file extension.
- The file contains only the following required fields:
- modelID
- did
- name
- sharedSecret
Device System Up Time "Unknown"
On the Device Summary page, in the Health information, if the System Up Time is displayed as "Unknown" this can mean there is a timing (or clock) issue on the device itself that is causing a negative up time to be recorded when Predix Edge syncs to the cloud. If you see this status, you should check your device for clock issues.
"Set Up Your Redirect URI" Error
If you try to login and receive the message: "You should not see this page. Set up your redirect URI," your session has timed out.
Solution
Re-enter your Edge Manager URL (for example, https://<your-tenant-id>.edgemanager.run.asv-pr.ice.predix.io), and sign in.
Error Messages
- Incorrect application URL
- Unable to get user token
- Unable to create session
- Unable to get tenant configuration
- Network connection to the authorization server for the tenant management service access token has timed out.
- Network connection to tenant management service has timed out.
- Tenant management service request has timed out.
- Request to the authorization server for the tenant management service access token has timed out.
- Unable to get tenant management service access token.
- Unable to get tenant configurations from the tenant management service.