About Predix Edge Manager Connectivity
Use Edge Manager Connectivity to establish connectivity between edge devices and the cloud over various networks, including cellular, fixed-line, and satellite communication.
In the left navigation pane, click Connectivity.
The Connectivity Dashboard displays information about VPN connection status, SIM state, SIM connections, and recent critical alerts.
In Edge Manager Connectivity, you can perform the following tasks:
- SIM List
- View and modify SIM lifecycle states.
- Modify data usage plans.
- View the current connectivity state for a SIM.
- View the current billing cycle's usage of the SIM.
- View SIM details such as ICCID, IP address, provider, and device ID.
- View alerts for SIM cards.
- Export the SIM list as a CSV file.
- Batch Update – update the rate plans and lifecycle states of multiple SIMs with one upload.
- VPN – view Virtual Private Network (VPN) connections and status associated with registered devices.