On the Commands page, you can choose to view commands in list view or tile view by clicking the corresponding icons in the top right of the page.
The following table describes the system defined commands for Predix Edge Manager, the applicable
platform, and the associated handler. The "Created On" and "Created By" columns display
additional information about custom commands, including the user who added the custom
command and the timestamp and date of when the command was added.
System-defined Default Commands for Predix Edge
System Commands
Description
Handler
Has Output?
Allow Third-Party Applications
Allows for the deployment of third party
applications. This may result in reduced security
for an edge device.
ApplicationManager
No
Reboot Device
Reboots the device.
Edge
No
Get Journal Log
Runs the system command \"journalctl"\ on
the device for the given parameters and returns
the output.
JournalLogs
Yes
Start Edge Application
Starts an Edge Application with the
specified Application ID.
ApplicationManager
No
Stop Edge Application
Stops an Edge Application with the
specified Application ID.
ApplicationManager
No
Delete Edge Application
Deletes an Edge Application with the
specified Application ID.
ApplicationManager
No
Set Polling Interval
Sets the duration of the polling interval,
which is used to schedule communications from the
device to the cloud.
Edge
No
Run ifconfig
Runs the system command \"ifconfig\" on the
device and returns the output.
Networking
Yes
Run top
Runs the system command \"top\" on the
device for one iteration and returns the
output.
Troubleshooting
Yes
Start Analytics Template
Starts the specified analytics template on
the device.
Analytics
No
Stop Analytics Template
Stops the specified analytics template on
the device.
Analytics
No
Delete Analytics Template
Removes the specified analytics template
and associated data map on the device.
Analytics
No
Get Edge Log
Retrieves the contents of the given log
file name and returns the output
Edgelog
Yes
List Edge Log
Returns a list of Edge log files
Edgelog
Yes
Note:
System-defined default commands cannot be edited or deleted.