Executing or Canceling Commands for a Single Device
You can use the Commands tab on the device details page to execute commands on a single device.
About this task
Procedure
- In the left navigation pane, select
.
- From the device list, click the device to run commands for, and click the Commands tab.The Commands page shows the command history for the device (if applicable).
- To execute the command, click Execute Command.
- In the Execute Command window, select the platform from the drop-down list, then select the command tile for the command to execute and click Next.Note:You cannot execute commands on devices with a status of "Created."
- In the Execute Command dialog box, enter a value for Timeout and select the unit of time (minutes, hours, or days).
- (Optional) If the command contains parameters, enter values for the parameters.Entering a parameter value is optional. Parameters are associated with the command, so different parameters apply to different commands, and these fields will vary.
- Click Execute.
- In the confirmation dialog box, click Close.
- To cancel pending commands, select the commands to cancel, and click Cancel Pending Commands.