Edge Core API

The Edge Core API allows users to interact with the system utilizing the same underlying functionality as Edge Manager or the Predix Technician Edge Console (PETC). The API is accessible from inside the device when logged into a terminal via a Unix domain socket. The API can be used for development purposes to manage applications, configure the network, perform host updates, retrieve logs, etc.

The API is not accessible from outside the device and is subject to change in future releases.