Device
Get OS Info
Gets the OS information of the device.
- Command: GET
-
http://localhost/api/v1/host/os
Curl examplecurl --unix-socket /var/run/edge-core/edge-core.sock \ http://localhost/api/v1/host/os
Table 1. Success 200 Field Type Description os_name String OS name os_version String OS version os_arch String OS architecture Success response example{ "os_name": "Edge OS", "os_version": "2.0.0-beta.8", "os_arch": "x86_64" }
Get Update State
Gets the state of an update.
State is kept for the most recent update attempt, so querying with an older update_identifier will return “NO UPGRADE OCCURRED”. Note: update_identifier is required because there is a brief lag between the start of an update and the actual upgrade process running. So if a client starts an update and then immediately tries to get the ‘state’ before the upgrade process has started, without the id they would get the state of the previous update, an incorrect result.
- Command: GET
-
http://localhost/api/v1/host/state?update_identifier=<identifier>
Table 2. Parameter Field Type Description update_identifier String Identifier of the update Curl examplecurl --unix-socket /var/run/edge-core/edge-core.sock \ http://localhost/api/v1/host/state?update_identifier=<identifier>
Table 3. Success 200 Field Type Description last_os_upgrade String State of the update associated with the identifier: "PASS", "FAIL", INPROGRESS" or "NO UPGRADE OCCURRED" Success response example{ "last_os_upgrade": "PASS" }
Reboot
Reboots the device.
- Command: POST
-
http://localhost/api/v1/host/reboot
Curl examplecurl --unix-socket /var/run/edge-core/edge-core.sock \ -X POST http://localhost/api/v1/host/reboot
Upon successful completion of the operation, the box will reboot.
Update
Updates the Edge OS and Edge Agent.
- Command: POST
-
http://localhost/api/v1/host/update
Table 4. Parameters Field Type Description update_identifier String An identifier associated with the update. Can be any string, as long as it is unique. file_name String Name of the Edge OS/Edge Agent update image file. Curl examplecurl --unix-socket /var/run/edge-core/edge-core.sock \ -X POST -H "update_identifier: <identifier>" -F "file=@<file_name>" \ http://localhost/api/v1/host/update
If the update is successfully applied, the device will reboot to complete the update.
Table 5. Error 4xx Field Type Description error_message String A description of the error encountered status_code Number The status code for the HTTP request Error response example{ "error_message": "<errorMessage>", "status_code": 500 }