Adding a Custom Command
You can add custom commands to manage devices.
Procedure
- In the left navigation pane, click Commands.
- Click .
-
In the Add Custom Command dialog box, enter the
information for the new command, then click Add.
- Display Name – Enter the name displayed to the user.
- Command – Enter the command in the following
format:
"command":<command>
- Handler – Enter the name of the package handler.
- Has Output – Select the check box if the command will produce output.
- Description – Enter a short description of the command.
- Platform – Select the platform (Predix Machine or Predix Edge) on which the command will run.
- Parameters Name – Enter the display name for the parameter, such as UNIT.
- Key – Enter the parameter that corresponds to the
parameter name, for example,
unit
. - Value – Enter the value that corresponds to the key.
- Editable – Select the check box to enable editing of command parameters.