VPN Management

You can perform VPN management on devices using Edge Manager.

To enable VPN management through Edge Manager, you must have a prepared environment with a server and client that are ready to communicate.

Select Connectivity > VPN to view Virtual Private Network (VPN) connections associated with registered devices.

The VPN Connectivity page displays the following information:

  • Status – Shows the connection status of the VPN client. When the check mark is green, it is connected. When the check mark is gray, it is disconnected.
  • Client ID – VPN client ID. Click the client ID to see details about the VPN.
  • Device ID – Unique number associated with the device.
  • IPv4 – VPN client IPv4 address.
  • IPv6 – VPN client IPv6 address.
  • Public IP – VPN client public address.
  • Server IPv4 – VPN server IPv4 address.
  • Server IPv6 – VPN server IPv6 address.
  • Connected Since – Timestamp for when the current connection was established.
Note:
The IPv4, IPv6, Public IP, Server IPv4, Server IPv6, and Connected Since fields are empty if the VPN is disconnected.

Enter "connected" in the search box to search for connected VPNs.