SIM Card Life Cycle
The following diagram displays the different states of the SIM card life cycle.

- Ready
- Unless otherwise specified when ordering, Ready is the default state for new SIM cards.
- When a minimum amount of data is passed on the SIM card, Ready transitions to Activated.
- Ready is a system state, and is not user-configurable.
- Activated
- Until the SIM card is in the Activated state, there is no billing.
- The Activated state allows the SIM card to pass data (subject to the associated rate plan).
- You can customize this state.
- Deactivated
- In the Deactivated state, the SIM card is no longer provisioned to pass data.
- You can customize this state.
- Purged
- Once the SIM card is in the Purged state, the SIM card cannot be reused.
- The Purged state is configurable by administrators only.
- Suspended
- When the SIM card exceeds the data usage of its associated plan, it is suspended.
- Not Available
- The Not Available state indicates an error with communication between the service provider and the SIM card.
If the Not Available state persists, contact support.