Assigning Predix Services to Devices

Assign Predix services like Time Series and Event Hub to devices.

Before you begin

You must configure services before you can assign them to devices.

Note:
You can have multiple services assigned to a device, but all assigned services must be bound to the same UAA service instance that is bound to your instance of Edge Manager so Edge Manager can issue a token with rights to that service instance.

Procedure

  1. In the left navigation pane, select Device Manager > Devices.
  2. In the device list, select, or filter, the devices to assign services to.
  3. In the upper right corner of the Device Manager page, click Device Operations > Assign Services.
  4. In the Assign Service dialog, select the services to assign, and click Assign.
    The operations for assigning services to the device ID are started.