Managing Edge Apps

About this task

Note:
The Edge Apps tab is displayed only for devices running on Predix Edge.

Procedure

  1. In the left navigation pane, select Device Manager > Devices.
  2. Click the name of the device with the edge apps you want to manage.
  3. Click the Edge Apps tab.
    The Deployment Schedule table shows a list of edge apps that are scheduled for deployment, along with the corresponding details and deployment status.
    The Applications table displays the edge apps that are deployed to the device and their status.
  4. Select the action to perform.
    • Click Start to start the edge app on the device.
    • Click Stop to stop the edge app on the device.
    • Click the trash can icon to delete an edge app from the device.
    The Status column shows the results of your action, and the Timestamp column displays the time and date the action was executed.
    If the device is offline, the Status is displayed as "pending" until the device is online and the action takes effect.
  5. (Optional) Click an Application ID to view the status of individual containers contained in the edge app.
    If there are errors associated with the container, click View in the Errors column to view the error message for the container.