Modify the settings for a specification

Procedure

  1. In the navigator, click Production.
  2. In the Folders list, select the resource type you want to work with.
    Tip:
    As more lists appear, select the appropriate resource until you find the one you want to work with.
  3. In the Displays panel, select an editor.
    The editor appears in the workspace, displaying the resource information.
  4. Click the Specifications tab, and then select a specification.
  5. If applicable, for the selected resource:
    1. Click Edit, and in the Name and Description fields, enter a new name or description.
    2. For a material resource, select a Material Use option.
    3. In the Quantity field, enter a new quantity.
    4. In the Unit of Measure field, enter a new unit of measure.
  6. Click Save.