Work Process Segment Specifications Tab

The Specifications tab allows you to add, modify, and delete equipment, material, and personnel specifications for the selected work process segment.

The following table describes the attributes specific to this resource type.

AttributeValueDescription
Specifications listUser-definedDisplays a list of associated equipment, material, and personnel resources that can be sorted by name or type.
Add EquipmentN/AClick to open the Universal Browser to select the resource that you want to use for the process.
Tip:
You can modify the quantity and unit of measure.
Add MaterialN/AClick to open the Universal Browser to select the resource that you want to use for the process.
Tip:
You can select how the material is used, and modify the quantify and unit of measure.
Add PersonnelN/AClick to open the Universal Browser to select the resource that you want to use for the process.
Tip:
You can modify the quantity and unit of measure.
Delete SelectionN/AClick to remove the selected specification.
Settings: Material UseUser-definedSelect the option that describes the material specification. Valid values are:
  • Produced
  • Consumed
  • Consumable
Note:
This options is available only when a material specification is configured.
Settings: QuantityUser-defined numeric valueSpecifies the required quantity for the resource.
Settings: Unit of MeasureUser-defined alphanumeric string (A-Z, a-z, 0 - 9) up to 20 charactersSpecifies the unit of measure, such as gallons, inches, tons.
Response Tracking: Property NameUser-defined alphanumeric string (A-Z, a-z, 0 - 9) up to 20 charactersDisplays the specification's property name.
Response Tracking: Class NameUser-defined alphanumeric string (A-Z, a-z, 0 - 9) up to 20 charactersDisplays the specification's class names, where applicable.
Response Tracking: Respond check boxN/ASelect this check box for each resource property whose resource actual property you want to track on an associated segment response.
Tip:
If you do not select this check box, you can still track resource properties on a segment response by using the AddResourceActualProperties call method in a workflow to explicitly add resource actual properties to a resource actual.