Work Requests
Work requests contain the information required to begin a production process.
Work requests are also associated with the events model. When a work request is created, any scheduled event is triggered in this section. It can be triggered automatically through a service provider from an external system, such as a master scheduler in a plant, or an alarm system, or manually through a user-defined workflow schedule.
Work requests can be created using the:
- Call Method activity in the Workflow model; or
- Work Requests resource type in the Production model.
The following topics describe the S95 Editor tabs and available attributes.