Work Request Properties
The Details tab offers general information about the selected work request.
Attribute | Value | Description |
---|---|---|
Name | Required; user-defined up to 50 characters | Specifies a display name for a resource. |
Description | User-defined up to 255 characters | Provides more information about a resource that a user may find helpful. |
The following table describes the attributes specific to this resource type.
Attribute | Value | Description |
---|---|---|
General Information | User-defined | Displays information about the work request. Information includes the associated work definition and the creation time and work type of the work definition. |
Location: Change | N/A | Click to open the Universal Browser to select the equipment that you want to use for this work request. The location is used to provide information about the valid equipment for the selected request. |
Location: Clear | N/A | Click to clear the equipment location. Note: This button is available only if an equipment location is currently set. |
Scheduling: Priority | User-defined numeric value | Specifies the order in which the work request will be performed. This setting can be used with automatic scheduling systems. For manual schedules, set the start and end times. Note:
Setting the priority is for internal use only; it does not affect the execution of a work request. |
Scheduling: Start Time | User-defined | Specifies the start date and time for the work request. This setting can be used with priority scheduling. |
Scheduling: End Time | User-defined | Specifies the end date and time for the work request. This setting can be used with priority scheduling. |
Status | System-defined | Specifies the status of the work request to provide information about a production event and to schedule workflows. Valid values are:
Note:
Changing the status can alter another production process. Status changes are signaled in the Events model. |