Work Request Parameters

The Requirements tab for the selected work request outlines all the information required to undertake a single production process. You can view and modify the parameter values for the current execution of the process.

You can also view and modify resource quantities for the material, equipment, and personnel resources in this process in a single location. Some resources are part of a larger, more generalized group or class. For these resources, you can select a more defined resource than the one that is currently defined as a requirement. For example, if the selected process indicates that it requires a mixer to perform a task, but the segment in this work request actually requires a specific mixer to complete the task at a particular time that this mixer is available, then you can indicate the specific mixer at this level.

The following table describes the attributes specific to this resource type.

AttributeValueDescription
Expand AllN/AClick to expand all the segment information for all the work requests' work definitions.
Collapse AllN/AClick to collapse the associations.
Earliest Start TimeSystem-definedSelect the start date and time for the segment.
Latest End TimeSystem-definedSelect the end date and time for the segment.
Work Parameters: Value fieldUser-definedSpecifies a parameter for the segment.
All requirements: Quantity fieldUser-definedSpecifies a parameter for the segment.
Select buttonUser-definedClick to open the Universal Browser to select a new resource requirement.
Note:
This button is available only if a class resource needs to be further defined.
Clear buttonUser-definedClick to remove the selected resource requirement.
Material Requirements: ConsumedUser-definedDisplays the output of the material resources when this work definition segment runs.
Material Requirements: ProducedUser-definedDisplays material required for the operation of the work request.
Material Requirements: ConsumableUser-definedDisplays information about the material resources that are consumed during the operation of the work request.