Work Process Segment Parameters Tab
The Parameters tab allows you to add, modify, and delete parameters that are specific to the selected work process segment.
Parameters in a work process segment are displayed with any associated work definition segment, where you can override the value.
If you add, delete, or modify a work process segment parameter, any associated work definition segments are also affected.
The following table describes the attributes specific to this resource type.
Attribute | Value | Description |
---|---|---|
List | User-defined | Displays a list of parameters for the selected resource that can be arranged by name, type, and so on, depending on the parameter. These parameters can be inherited from another resource or created for the current resource. |
Add Parameter | N/A | Click to add a new parameter. |
Delete Selection | N/A | Click to remove the selected parameter. |
Name | User-defined alphanumeric string (A-Z, a-z, 0 - 9) up to 20 characters | Specifies a display name for the selected property. |
Description | User-defined alphanumeric string (A-Z, a-z, 0 - 9) up to 20 characters | Provides more information that a user may find helpful. |
Data Type | System-defined | Specifies the data type of the parameter. This parameter cannot be changed if it is inherited from another resource. |
Value | User-defined alphanumeric string (A-Z, a-z, 0 - 9) up to 20 characters | Specifies the value for the selected data type. Valid values depend on the selected data type. |
UoM (Unit of Measure) | User-defined alphanumeric string (A-Z, a-z, 0 - 9) up to 20 characters | Specifies the unit of measure for the data type, such as gallons, inches, tons. |