Work Process Segment Details Tab

The Details tab offers general information about the selected work process segment.

You can change the name and description of this resource.
Attribute Value Description
Name Required; user-defined up to 50 characters Specifies a display name for a resource.
Description Required; user-defined up to 255 characters Provides more information about a resource that a user may find helpful.

The following table describes the attributes specific to this resource type.

AttributeValueDescription
Location: ChangeN/AClick to open the Universal Browser to select the equipment that you want to use for the process location. It identifies the associated element of the equipment hierarchy model. It may also define the scope of the process segment definition, such as the site or area it is defined for; therefore, it is not intended for locations outside of the scope.
Location: ClearN/AClick to clear the equipment location.
Note:
This button is available only if an equipment location is currently set.
Set as Master check boxN/ASpecifies whether the process segment is a master segment.
Process Duration: DurationUser-defined numeric valueSpecifies the resource's duration. The duration can be defined at any level of the process. Duration is not inherited through an association with another resource.
Process Duration: Unit of MeasureUser-defined alphanumeric string (A-Z, a-z, 0 - 9) up to 20 charactersSpecifies the duration's unit of measure, such as gallons, inches, tons.
Work Type System-definedSpecifies the work type to describe the category of work that the work process segment is associated with. Valid values are:
  • Production
  • Maintenance
  • Quality
  • Inventory
  • Mixed
  • Unspecified
Workflow: ChangeN/AClick to open the Universal Browser to select the workflow to associate with this process segment. It identifies the associated element of the workflow hierarchy model.
Workflow: ClearN/AClick to clear the workflow association.
Note:
This button is available only if a workflow association is currently set.