Work Process Segment Work Data Tab

The Work Data tab for the selected work process segment allows you to add, modify, and delete work data classes.

Work data classes associated with a work process segment are inherited by a work definition segment when it is associated with the work process segment. Each class adds its collection of properties to the work data associated with the work process segment.

For more information, see Work Data Classes.

The following table describes the attributes specific to this resource type.

AttributeValueDescription
Class ListUser-definedDisplays a list of work data classes that can be sorted by name.
Add ClassN/AClick to open the Universal Browser to select the work data class that you want to use for the process segment.
Note:
You can use up to 50 work data classes per work process segment. The options available to you are in bold.
Delete SelectionN/AClick to remove the selected work data class.
Required ClassUser-definedSelect this check box to ensure that the work data for a work process segment is automatically applied to segment responses.
PropertiesUser-definedDisplays all the properties configured on the selected work data class.