Add specifications to a process segment
Before you begin
Note:
You must create equipment, material, and personnel resources before you can add them as specifications.
Procedure
- In the navigator, click Production.
- In the Folders list, select the resource type you want to work with.Tip:As more lists appear, select the appropriate resource until you find the one you want to work with.
- In the Displays panel, select an editor.The editor appears in the workspace, displaying the resource information.
- Click the Specifications tab.
- If required, add the following resources:
Click... To add... Add Equipment an equipment or location resource Add Material a material resource Add Personnel people or personnel class resources The Universal Browser appears. - Locate and select the resource you want to add as a specification, and then click OK.
- In the Name and Description fields, enter a name and description for the specification.
- Optional: In the Quantity and Unit of Measure fields, enter a quantity and unit of measure.
- For material specifications, select a Material Use option.
- Optional: Select the Response Tracking check box for each resource property you want to track on a segment response.
- Click Save.