Production Event Source Properties

You can use event source properties to monitor particular events related to conditional events or workflow schedules.

Note:
You can only bind parameters to property values of similar data types.

Common Event Source Properties

The following table describes the common properties available for each event source.
PropertyData TypeDescription
IdGUIDUnique key that identifies the event definition in the data model.
NameStringDisplay name of the event definition resource.
DescriptionStringAdditional information related to the event definition resource.
TimestampDateTimeThe actual UTC time that the event occurred.
EventNodeAddressEventAddressThe Directory Address of the event that occurred.
EventTypeStringThe .NET type of the event occurrence.
KeepArchiveBooleanIf the event associated with the workflow schedule is maintained in history by the event manager, this is True.