Evaluation of Condition Expressions
The Trigger Settings tab allows you to determine when the configured condition expressions will be evaluated. The results of these evaluations determine whether or not the event can run.
The following table provides more information on the outcome of selecting a trigger type:
Trigger | Value | Description |
---|---|---|
Trigger only on Variable Value changes | System-defined | Evaluates the expressions when a variable changes. These changes can occur through a bind to external data or to an attribute of another event. |
Trigger on Event or Variable Value changes | System-defined | Evaluates the expressions when a variable changes or when the selected event trigger is signaled. |
Trigger only on Event | System-defined | Evaluates the expressions only when the selected event trigger is signaled. |
Set Event Trigger | N/A | Click to open the Configure Event Trigger dialog box and select the appropriate event trigger. |
Clear | N/A | Click to clear the selected event trigger. |