Properties and Attributes of Condition Events
The Details tab offers general information about the selected condition event.
You can change the name and description of this resource.
Attribute | Value | Description |
---|---|---|
Name | Required; user-defined up to 50 characters | Specifies a display name for a resource. |
Description | User-defined up to 255 characters | Provides more information about a resource that a user may find helpful. |
The following table describes the attributes specific to this resource type.
Attribute | Value | Description |
---|---|---|
State | User-defined | Indicates if the event is enabled or disabled. |
Event Summary | N/A | Summarizes the current status of a conditional event, as well as when it will be used. |
Variables Summary | N/A | Displays all variables associated with the selected event, if any. Variables can be bound to properties of other production resources. |
Condition Expressions Summary | N/A | Displays all expressions associated with the selected event, if any. |