Time Events
Time events can be set by time span or by calendar, and they can be either single or recurring events.
Events always fire against the local server time. However, the following exception applies during daylight saving time (DST) change.
Example: When time interval is configured in Days (or) in combination of Days and
Hours.
- When the clock is set back in autumn, an event set for 2:30 A.M. fires only once when the time is reached for the second time (after DST ends).
- When the clock is moved forward in spring, an event set for 2:30 A.M. fires once at 3:30 A.M. on the first day (which would have been 2:30 A.M. before the time change), and then fired again at 2:30 A.M. the following day.
Example: When time interval is configured in Hours.
- When the clock is set back in autumn, an event set for a particular time, such as 1:30 A.M. fires twice - once at the original time of 1:30 A.M., and then once again when that time reaches 1:30 A.M. for the second time.
- When time interval is configured as Hour(s): When the clock is moved forward in spring, an event set for 2:30 A.M. fires at 3:30 A.M. on the first day (which would have been 2:30 A.M. before the time change), and then at 2:30 A.M. the following day.
Note:
When you change the timezone in your system, make sure to restart the Proficy
Workflow Client to reflect the correct event time in the Event
Editor.
Resource Properties
The following table describes general information on properties for user-defined
resources:
Attribute | Value | Description |
---|---|---|
Name | Required; user-defined up to 50 characters | Specifies a display name for a resource. |
Description | User-defined up to 255 characters | Provides more information about a resource that a user may find helpful. |