Create variables for a condition event

Procedure

  1. In the navigator, click Events.
  2. In the Folders list, select the resource type you want to work with.
    Tip:
    As more lists appear, select the appropriate resource until you find the one you want to work with.
  3. In the Displays panel, select an editor.
    The editor appears in the workspace, displaying the resource information.
  4. On the Variables tab, click Add.
    Tip:
    To permanently remove a variable from the event, select the variable, and then click Delete.
  5. In the Variable Name field, enter a name.
    Note:
    The variable name must be alphanumeric and must not contain spaces.
  6. Select one of the following options:
    Select...Then...
    Bind variable to external data
    • Click Configure Data Item. The Configure Variable Data Source dialog box appears.
    • Configure the data source.
    • Click OK.
    Bind variable to an attribute of the Event Trigger
    Note:
    This option is available only if a trigger event has been set.
    • Select an attribute.
    • Enter a default value.
    Variable represents a constant value
    • Select a data type.
    • Enter a value for the data type.
  7. Click Save.