Set up class-based events
You can bind class properties to event variables so that an event can detect a property change in any equipment to which that class has been added.
About this task
Note:
This does not allow you to detect property changes in equipment properties where that class has been used as the Type.
Procedure
- In the navigator, click Events.
- In the Folders list, select the resource type you want to work with.Tip:As more lists appear, select the appropriate resource until you find the one you want to work with.
- In the Displays panel, select an editor.The editor appears in the workspace, displaying the resource information.
- On the Trigger Settings tab, select either:
- Trigger only on Variable Value changes
- Trigger on Event or Variable Value changes
- Click the Variables tab, and then click Add.
- Configure the variable as follows: