GE Historian Event Source Properties
You can use event source properties to monitor particular events related to conditional events or workflow schedules.
Note:
You can only bind parameters to property values of similar data types.
Common Event Source Propeties
The following table describes the common properties available for each event source.
Property | Data Type | Description |
---|---|---|
Id | GUID | Unique key that identifies the event definition in the data model. |
Name | String | Display name of the event definition resource. |
Description | String | Additional information related to the event definition resource. |
Timestamp | DateTime | The actual UTC time that the event occurred. |
EventNodeAddress | EventAddress | The Directory Address of the event that occurred. |
EventType | String | The .NET type of the event occurrence. |
KeepArchive | Boolean | If the event associated with the workflow schedule is maintained in history by the event manager, this is True. |