Equipment Event Source Properties
You can use event source properties to monitor particular events related to conditional events or workflow schedules.
Common Event Source Properties
The following table describes the common properties available for each event
source.
Property | Data Type | Description |
---|---|---|
Id | GUID | Unique key that identifies the event definition in the data model. |
Name | String | Display name of the event definition resource. |
Description | String | Additional information related to the event definition resource. |
Timestamp | DateTime | The actual UTC time that the event occurred. |
EventNodeAddress | EventAddress | The Directory Address of the event that occurred. |
EventType | String | The .NET type of the event occurrence. |
KeepArchive | Boolean | If the event associated with the workflow schedule is maintained in history by the event manager, this is True. |