WriteWorkParameters (IProductionRuntime)
Writes the value of specified work definition segment parameters to a process segment.
Note:
In the Configure Method dialog box, click Next to select a work data class and its properties you want to write. You can select all properties or a subset. Each property you select displays as an input parameter on the activity configuration panel.
Inputs | Data Type | Description |
---|---|---|
Requirement ID | String | Specifies the ID of the segment requirement to write the parameter values to. |
Work data input parameters | Dependent on each parameter's data type | Specifies the value for each work definition segment parameter to write to the process segment. |